Tool/software:
Dear TI Guys:
When Gauge entered the shutdown mode by AUTO SHIP Time, whether it returns to normal if only voltage at PACK pin > VSTARTUP?
How to Config. parameters that it can return to normal when press the shutdown pin16?
5.4.3 Time Based Shutdown
The device can be configured to shut down after staying in SLEEP mode without communication for a preset
time interval specified in the Auto Ship Time. Setting the PowerConfig[AUTO_SHIP_EN] = 1 enables this
feature. Any communication to the device will restart the timer. When the timer reaches the Auto Ship Time,
the time based shutdown effectively triggers the MAC shutdown command to start the shutdown sequence.
The device returns to NORMAL mode when voltage at PACK pin > VSTARTUP.