Other Parts Discussed in Thread: BQ79616
Tool/software:
Dears CC,
We have run the power supply BIST at start up in the BQ79616-Q1 device and found PWRBIST_Fail Bit =1.
We further diagnosed and checked all the bits from FAULT_PWR1 and FAULT_PWR2 registers and found all bits are 1 accept RSVD bits.
- CVSS_OPEN =1
- DVSS_OPEN =1
- REFHM_OPEN =1
- CVDD_UV =1
- CVDD_OV =1
- DVDD_OV =1
- AVDD_OSC =1
- AVDD_OV =1
- RSVD =0
- PWRBIST_FAIL =1
- RSVD =0
- REFH_OSC =1
- NEG5V =1
- TSREF_OSC =1
- TSREF_UV =1
- TSREF_OV =1
as per the data sheet of BQ79616-Q1, page 85
" The power supply BIST forces a failure and ensures the diagnostic path triggers the fault accordingly. A failure
on the BIST run indicates a diagnostic path is unable to trigger in a fault condition. To further examine which
path is unable to indicate a failure, host can set the DIAG_PWR_CTRL[BIST_NO_RST] = 1. This bit disables the
reset step during the BIST run. Re-start power supply BIST with this option enabled. At the end of the BIST run,
examine the FAULT_PWR1 and FAULT_PWR2 registers. Any register flag that remains 0 indicates it is unable to
flag a failure."
Please suggest what are the possible reasons which makes PWRBIST_FAIL = 1.
thanks and regards
Subhash Dhyani