This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65988: How to use the TM4C123G LaunchPad Evaluation Board to program and debug TPS65988DH based system

Part Number: TPS65988

Tool/software:

I purchased a TM4C123G LaunchPad Evaluation Board for the purpose of programing and debugging a TPS65988DH based system.  I have connected the following highlighted signals on the TM4C123G LaunchPad Evaluation Board to the TPS65988DH based system.  

The TIVA board as it is received does not work to communicate with the TPS65988DH based target.  This is the USB to I2C/SPI Adapter settings

When connecting the TIVA board to the PC, no added com ports come up.  Should this board be compatible with the drivers that are installed with the EVM?

Best regards,

David