Other Parts Discussed in Thread: DAC80501, TPS923652
Tool/software:
Hi TI,
First of all, I apologize that the part number in the post is not appropriate.
As far as I know, most LED driver products are unable to output low currents due to analog dimming.
I am looking for an LED driver with a maximum output of 2A or more that also allows for low level (0~10%) analog dimming.
Then I checked the SLVA471 (How to Use Analog Dimming With the TPS6116x) document and would like to ask a question related to it.
1. What is the minimum current (greater than 0) that can be output with analog dimming?
2. I ultimately want a driver with 0-2A output. If you have a suitable IC or technical document, please introduce it.
P.S: I plan to supply analog dimming with DAC80501.
Thank you.