Tool/software:
Greetings TI,
I am using TPS259823ONRGET Efuse IC with 5V input with current limit of 2A.
the circuit flow is Battery efuse circuit connected to load
my load maximum gives 0.5 Amps even though when i connect efuse circuit to load and then battery is supplied power to it the circuit is shutting down. Can i get any explanation on why it is happening. what can i do to avoid this.
Thank you in advance.
K Bindhu