This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ77207: Cell Balancing

Part Number: BQ77207

Tool/software:

Can the BQ77207 IC perform cell balancing? If so, can this feature be disabled or enabled when ordering? 

  • Hello,

    The BQ77207 IC does not support cell balancing.

    If you are looking for cell balancing, I suggest the BQ77915

    • Scalable cell count from 3 series to 20 series or more
    • Overvoltage: 3 V to 4.575 V
    • Undervoltage: 1.2 V to 3 V
    • Current protection
    • Smart passive cell balancing removes cell-to-cell imbalance

    I would also suggest the BQ76907:

    • Battery monitoring capability for 2-series to 7- series cells
    • Extensive protection suite including voltage, temperature, current, and internal diagnostics
    • Needs host for cell balancing

    Best regards,

    Thomas Rainey