Tool/software:
Hi
I am trying to use quick-start to control the output of the buck converters in a TPS65941111EVM.
Both stacked EVMs are in a 1+1+1+1 configuration.
I was able to connect the EVM through I2C to the GUI (I closed GPIO2,SDA2/SDO; GPIO1,SCL2/CS, selected closed the jumpers for master and slave on their respective EVMs, and provided 3.3V to VSYS through an external power supply; I also set J47 to VCCA), but the GUI displays the message "Duplicate device names (or) invalid name found !" whenever I scan for devices.
I have also tried to write the registers individually, but even if I set the BUCK EN bits, I get no output.
What can I do to access quick-start?
Thank you.