Tool/software:
Hi,
I am currently looking to use the LM5069 as a "40V 8A Efuse". In our application there are moments when current can flow from the output to the input while LM5069 is disabled
I was testing this on the evaluation board and it does not seem to work. Reason being the power supply goes into current limit at 10mA and using a thermal camera I can see the LM5069 is starting to heat up
I am wondering if this is due to the protection diode connecting the output to the gate pin internally to the IC?
Do you have any other recommendations of other parts that I could use that allows for current to flow from the output to the input through the body diode of the external mosfet while the driver is off
also giving overcurrent and short circuit protection when in normal operation (current flow VIN to Vout)?
Thanks for all the help,
Visaacan