This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34Z100-G1: Can I manually change the Update Status in the Data Memory Gas Gauging section?

Part Number: BQ34Z100-G1
Other Parts Discussed in Thread: BQSTUDIO

Tool/software:

I am having difficulty getting the Update Status to change from 06 to 04. I am attempting to follow SLUA925 for my 7000 mAh 3S2P battery pack. In bqStudio, with the battery pack being read, I click the command IT_ENABLE to send a 0x21 command, followed by the RESET 0x41 command. I am unable to get the Update Status to switch over from 06 to 04. I am able to double click in the Update Status box and manually type in 04 and Write_All. Will this accomplish the same goal?