Tool/software:
Now we have encountered a situation where the chip output cannot be turned off under light load. In the figure, input POWER: 3.0V and output VCC_m: 3.3V
We found the following phenomenon when using TPS63900:
When a load of only a few μ A is connected to VCP_M, even if VCP_CTL2 is set low, there is still a voltage of about 2.6V on VCP_M, and the current at the POWER input terminal will increase by about 10uA. (If VCP_M is turned off at this time, the chip output can be turned off)
Please help analyze where the problem is