This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24133: Queries about this part: BQ24133RGYR

Part Number: BQ24133

Tool/software:

My query is about the BQ24133RGYR IC. I need details about its current availability and supply confirmation.

I am planning to use it for charging with the following specifications:

  • Input: 15V
  • 3 cells, each with 4.2V
  • Charging and discharging current: 1A
  • Overcurrent and overvoltage protection
  • Auto cut-off for overcharging
  • Temperature monitoring

Most importantly, I need constant voltage and current for charging. These are my requirements.

I checked the BQ24133EVM-715-15V evaluation board for testing my requirements, but it is probably not available for sale online.

Additionally, I do not have the circuit layout and schematic references for the IC-based circuit.

Please provide contact details for distributors and dealers in India for this part.

If it is not currently available, please share information about new equivalent parts and recently released products, as we are planning to use this IC for the next 10 years.

Furthermore, please share the schematics or circuit diagram for verification of my requirements.