Other Parts Discussed in Thread: BQ25185, BQSTUDIO
Tool/software:
Hello I'm getting ready to go through the learning cycle process.
Our current design utilizes a solar and a bq25185 charger...with cutoff currently set to 30mA.
I've been told the current expectation of the solar panel is around 50mA at best. We're using an inr18650-35E 4p pack, with a cutoff current of (68mA per cell-->272mA for the pack) at the standard charge 4.2V, 1700mA per cell->6800mA for the pack)
We are nowhere near the standard charge currents-I believe this is called trickle charging. Will this gauge still work at these low current levels.
How should I set the charge term taper current mentioned here:
Achieving The Successful Learning Cycle (tij.co.jp)
The learning process was going to be performed charging provided by a power supply. But the fielded battery will utilize solar panel charging only.
Thanks,