This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ77915: CHG pin oscillating

Part Number: BQ77915


Tool/software:

Hi,

My design with the BQ77915 is the following. I am not using the CHG and DSG option, just the balancing;

I am observing strange behaviour on CHG pin (DSG is also always low..).

I am not using temp sensor, so it should not be a temperature error.

The only errors left that have both CHG and DSG OFF are:

- OW: no, I checked voltage difference

- OCC: also no, I have (VSRP – VSRN) = 40mV

-OCD1, OCD2, SCD: I am in charge so it should not be this.

What am I missing ?

Regards