This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2940QML: 5962-8958703XA or LM2940GW5.0/883

Part Number: LM2940QML


Tool/software:

Hello,

I want to know if the 5962-8958703XA or LM2940GW5.0/883 parts are hermetically sealed. I can't find anywhere on the datasheet suggesting that it is but the mil doc states that this PN is. The NAC package drawing for this part also does not state that it is hermetically sealed.

The .mil doc STANDARD MICROCIRCUIT DRAWING BULLETIN (5962-89587) states  "The lead finish shown for each PIN representing a hermetic package is the most readily available from the manufacturer listed for that part. If the desired lead finish is not listed contact the vendor to determine its availability."

The doc references the table that lists the following part numbers:

Standard microcircuit drawing

PIN 1/ Vendor CAGE number Vendor similar PIN 2/

5962-8958701EA 3/ LM2940J-5.0/883

5962-8958701MA 3/ OM2940-5SRM/883B

5962-8958701NA 3/ OM2940-5N5M/883B

5962-8958701UA 3/ OM2940-5STM

5962-8958701XA 3/ LM2940WG-5.0/883

5962-8958701YA 3/ LM2940K-5.0/883

5962R8958702VXA 3/ LM2940WG5.0RLQV

5962R8958702V9A 01295 LM2940-5.0 MDE

5962-8958703XA 01295 LM2940GW5.0/883

5962R8958704VXA 01295 LM2940GW5.0RLQV