This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS92610-Q1: Temperature effect on output current

Part Number: TPS92610-Q1

Tool/software:

Dear TI team,

I am working on a project that is going to use the TPS92610-Q1, and I need to know the effect produce by the temperature. I mean, I need either to math or simulate the effect that the temperature will produce over the IC, to know the possible increase or reduction of current due to the temperatures at -40C, 25C, 70C and 85C. However, I see no any information about this, I tried to simulate the temperature spec in simetrix but the SPICE model didn't support it, so I would like to know if it would be a manner to calculate this increase or reduction.

As this moment, the current is set at 200mA so we assume this consume is at 25C but we need to know how much the current will increase at 70C and 85C, and how much the current will decrease at -40C.

Best regards