Tool/software:
Hello,
I am experiencing an issue with the bq25125 battery charger IC. When I set the charge current (ICHRG) higher than 70mA, I receive an error status with STAT_0 and STAT_1 both set to 1 (binary 11). At 70mA, the system works fine.
Here are the key settings I am using:
- Reset the bq25125.
- Set ILIM to 200mA.
- Set CE to 0 (Charge Enable).
- Set the MRRESET to 5 seconds.
- Configure SYS VOUT to 2.5V.
- Disable VINDPM and MRREC.
- Set ICHRG to 70mA (works fine) or higher (causes the error).
Despite these settings, increasing ICHRG beyond 70mA results in an error status. Could anyone provide insights or suggestions on what might be causing this issue and how to resolve it?
Thank you for your help!