Tool/software:
Hi support team,
I am using LM27761DSG under the following conditions, but it goes into PFM mode.
Vin : 5V
Vout : -5V
Iout : 15 ~ 50mA
Application : Strain Input Module
Are there any devices that do not have a light load mode and have an LDO output?
I do not want to use a switching regulator because I want to suppress noise generation.
Regards,
Dice-K