This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34Z100EVM: BQ34Z100EVM

Part Number: BQ34Z100EVM
Other Parts Discussed in Thread: EV2400, BQSTUDIO

Tool/software:

HI,

1. I am using a BQ34Z100EVM Board with Arduino UNO and write the code wire library in arduino to take i2c data but I don't receive any data in arduino

2. Arduino is also not connected with BQ Studio.

3. Can I use Bq34z100evm without EV2300 or EV2400 to get the battery health .

4.How I can check the BQ34z100EVM board firmware is loaded properly 

Please suggest how I can make connections and firmware for the Arduino to get the battery status and battery health from the BQ34Z100EVM BOARD with 24V battery