This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65994AE: We tested the FV at GRL, and there was a test item of 3.3.6 & 3.7.2.2

Part Number: TPS65994AE

Tool/software:

Hi Raymond,

Item : eGFX_AMD and eGFX_NVIDIA
Detail : SUT will shows yellow bang when power on the system.

refer to below from Raymond.

eGFX: Looks like there be some correlation between the PDO power and their external GPU having issues.

I’ve attached PD logs captured for each of these issues. I recommend following up on e2e for each of these issues with the attached logs for further debug.

about Log as attach file:

2450.Clevo_eGFX_PortA_PD_Logs.zip

Thanks~

Marty