Other Parts Discussed in Thread: TPS25961, TPS2596, , TPS1641
Tool/software:
Hi
I'm using the TPS259533DSGT for currents as low as 100mA and the only thing I noticed was the trigger level was not within tolerance of the TPS259533.
As I understand it, the TPS259533 is set to function between 0.5A - 4A because of the linearity of the correlation between the resistor value and the current limit. The correlation starts to be linear from 0.5A and the current is limited to 4A by the internal FET.
So technically, I should be fine using it below the recommended 0.5A? Or is there another reason for the lower current limit? If so, what can be the issue with using it below 0.5A?
KR