This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TL494: Short circuit protection alternative design

Part Number: TL494

Tool/software:

Hello.

I will design a buck converter that can provide up to 8A current at 5 volts. I want to use TL494 for my design but I have some questions. In the typical application circuit the load is floating and short-circuit sense resistor is 100 mOhms which will dissipate a lot of power. How can I have short-circuit protection without making the load float and dissipating power on sense resistor?

Thank you.

Datasheet Link: https://www.ti.com/lit/gpn/TL494