Tool/software:
Hello experts,
I hope to find what the minimum Vin LV14360 can intake for load of Vout=24Vin & Iout=1A (max).
On datasheet it says max duty is 90% with fsw=200kHz, but I assume at 600kHz, max duty would be different.
I couldn't find any info/graph on max duty at fsw=600kHz, or min on-time, etc..could I ask what it would be?
In summary I have 2 questions,
1. What is max duty cycle at 600kHz?
2. What is the frequency that can support maximum max duty possible? (ex. If fsw=100kHz can support even larger max duty, please let me know.)
Thank you in advance for your support.