Other Parts Discussed in Thread: BQSTUDIO, BQ27426, EV2400
Tool/software:
Hi,
i am using BQ27Z746 for my battery application. i have to read the battery percentage and to trigger an alarm for OV, OC, UV, UC protection. Below are my queries, please clarify.
Q1. what are the registers need to be initialized for the above application and where can i find the specific register address?
Q2. Can i set the parameters like Design capacity, Design Voltage, Terminating voltage etc. without BQSTUDIO by directly writing using I2C write function during initialization? Please refer the attached image.
Q3. which document shall i refer to get the proper register address and its explanation regarding the purpose it is being used?
Q4. Do i need Evaluation kit to use BQSTUDIO or it can be interfaced to BQ27Z746 using jumpers on my project PCB?
waiting for the answers........
Thanks,
Sumit.