Other Parts Discussed in Thread: TPS61040
Tool/software:
Hello,
during the temperature evaluation of the TPS61040Q1 actual device, a uncertain behavior of the IC was observed.
In this situation, the efficiency drops sharply ant the output voltage is almost equal to the input voltage.
Description of the test setup and conditions:
In the design, we boost the input voltage (~5.5V) to an output voltage of about 26 V. The expected load current is ~6 mA. At ambient temperature (25 °C) everything works as expected.
In our test scenario our product is placed in a climate chamber where the ambient temperature is around 55 °C.
After detecting a problem with the converter, we monitored the temperature of the IC housing with a sensor on the housing.
The temperature measurement shows the following result:
The temperature profile shows that at a temperature of 80.5 °C the converter switches to a mode in which the efficiency decreases rapidly and therefore a lot of power loss and corresponding heat is produced.
This can be seen from the rapid rise in temperature after this point.
In this mode, the following signal curve can be measured on pin 1 (SW).
How can this behavior be explained, since the data sheet specifies an operating temperature of up to 125 °C?
Could you please help on this?