Tool/software:
hello
I want to implement a design from 3.5V to 2.2V with LM1084_ADJ, load current is 2A 。
Please help to check whether the SCHMATIC is correct ,thanks。

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello there,
Some notes I can give is that your resistor values a bit off. The formula to calculate: Vout = Vref(1+ R2/R1). In this case, R1 = 121Ω and R2 = 159Ω and we can ignore the Iadj current since R1 is greater than 100Ω. The current Iadj from the adjustment terminal introduces an output error. But because it is small (120 uA max), it becomes negligible when R1 is in the 100 Ω range. These resistor values results in Vout = 2.89V.
My work:
Vout = 1.25(1 + (159/121)) = 2.89V
To get your desired 2.2V, you would have to switch your R2 (159 Ω) to 92 Ω.
Work:
Vout = 1.25(1 + (92/121)) = 2.20V
Your capacitors at the input and output are sufficient and meet datasheet specifications.