This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP5862: II2C doesn't work

Part Number: LP5862
Other Parts Discussed in Thread: LP5860

Tool/software:

Hi,

I am using the LP5862 in the following circuit:

I try sending the I2C message 0x43 and try writing 0x00, but no acknowledge bit comes across as the address byte is sent. 

The IC is on, since VCAP pin has a voltage of 1.78V. 

I tries sending exactly the same message on the evaluation board of LP5860, and the acknowledge was successful as seen bellow:

Any suggestions?

Best regards

Ehsan