This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS1H200A-Q1: TPS1H200A-Q1

Part Number: TPS1H200A-Q1

Tool/software:

Good morning, i'm using TPS1H200A to drive a solenoid of about 500mA 24V. the configuration in showed in the schematic

The TPS don't work (input signal to 3.3V but output dont't swing at  VIN =24V). To solve the issue i need to reduce the value of R20 to 100ohm instead of 1K suggested by datasheet (see chapter 7.3.6.5 Reverse-Current Protection)

It's correct?

Regards

Paolo