Other Parts Discussed in Thread: BQ34Z100
Tool/software:
Dear TI specialist, dear community,
I am working with the BQ34Z100-R2 chip to gauge a 100 Ah 12V batteries. I have successfully trained the chip and am achieving good SOC accuracy.
Our batteries are meant for outdoor use and are shipped in watertight and insulated cases, which should not be opened by the customer or any personnel.
We are using 15 A to charge the battery, and during the charge, the chip temperature increases to 60°C. I have incorporated a passive cooler (10x10x10 mm), which has reduced the temperature to somewhere between 40°C to 50°C during charging at 15 A. Even though the chip temperature is well within the specified operating range, I personally find it a bit high.
Is such a high temperature of the chip normal during charging?
What would you recommend to keep the temperature lower, especially if we decide to allow for higher charging currents, such as 30 A or even 50 A, in the future? Any PCB design recommendations? We would prefer to keep the temperature regulation passive, so adding an active cooler would not be the preferred solution.
Thank you very much!
Best regards,
Vojtech Krcmarsky