Other Parts Discussed in Thread: BQ40Z50, BQ25672EVM, BQ25672, EV2400, BQ25798, BQ25710
Tool/software:
Hello,
we are working on a Battery Management System to be set up in our Robots and Smart home devices to be designed with these specifications:
- -1 to 4 S 18650 Lithium Ion Batteries (each cell capacity is 1500mAH).
- -Has dual power input: Solar input/MPPT, USB C/PD Charger support.
- -Cell Battery Pack Manager and Protection.
- -Battery Monitoring - Fuel gauge to monitor the health and the remaining capacity percentage.
- -The Fuel gauge IC and the charger should be communicated with each other to charge and maintain the battery health.
- -The MCU should communicate with both the Fuel gauge and the charger IC to monitor the current state ( charging, discharging). Also, monitor the battery health and the remaining capacity percentage.
From that point, we make an initial selection as Following:
- BQ40Z50EVM-561 to be used to understand the concept of the Fuel gauge IC BQ40Z50.
- BQ25672EVM to be used to understand the concept of the charger IC BQ25672.
- EV2400 evaluation kit to set up the required parameter from the PC.
"Kindly note that we decide first to use a dev kit from the recommended ICs to be familiar with them then we will design our PCBs based on the ICs we used in the dev kits"
So, we need an assist to ensure that this selection is suitable for our applications and the devkits also.