This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5148: Design to generate 36VDC@5A

Part Number: LM5148
Other Parts Discussed in Thread: LM5145, LM70860

Tool/software:

Hello,

I am going to Design the DCDC power supply and below are the requirements

  • Input voltage : 48VDC (41 VDC to 57VDC)
  • Input current : 4.1A
  • Output Voltage : 36VDC
  • Output current : 5A

Kindly provide the sugestion whether LM5148 is the right selection OR any other IC is suitable for thgis application.

Regards,

Alpesh