Part Number: UCC28C59
Other Parts Discussed in Thread: UCC2897A
Tool/software:

Hi,
We are using UCC28C59 for a 60W Forward Converter on Simetrix.
Some questions or clarifications about this reference:
- Based on datasheet table 7.1, to obtain 100kHz switching frequency, we need to set Rt = 3.05kR and Ct = 2.2nF. Right ?
- We meet some trouble on output pin, control loop is updated one time on two (see attached screeshoot), first pulse is at his maximal value and the second to the minimal value.
We suspected it may occur due to wrong pole and zero placement. Do you have some application note to set compensator value (we based our compensator value on slva662).
BR,