Other Parts Discussed in Thread: LM76005,
Tool/software:
Hi team,
I'm testing source mode using PP5V on the EVM. So I supplied PD power over J2 connector(20V) and didn't connect any BQ devices on the EVM.
I wanted to charge my iPhone using PP1 path (5V 3A) internally generated by LM76005 but it didn't show what I expected.
When I read 26h, it said "3h = PP3 switch enabled (system input)" So, It seems like the iPhone is keep working as a source instead of Sinking.
So I tried the SWSr command, but the result was same that the iPhone is keeping its status as Source.
Can you help what I should do to keep TPS25751EVM as a source mode?
Please see below PD log and json files.
PD log when SWRs.csvhttps://e2e.ti.com/cfs-file/__key/communityserver-discussions-components-files/196/PD-log-when-SWRs.ccgx3
{ "questionnaire": { "device": "TPS25751", "answers": [ null, 1, 0, 1, 1, 0, 3, 0, 0, 1, 1, null, 0, 0, 0, 0, 0, 0, 0 ], "vendorId": "0000", "productId": "0000", "version": "1.0.0.2" }, "configuration": { "data": { "selected_ace": [ { "register": 6, "data": [ 0, 0, 0, 0, 0, 0, 0, 0 ] }, { "register": 22, "data": [ 0, 0, 0, 0, 0, 0, 0, 16, 0, 0, 3 ] }, { "register": 40, "data": [ 2, 0, 47, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0 ] }, { "register": 41, "data": [ 114, 80, 144, 3 ] }, { "register": 50, "data": [ 1, 168, 42, 44, 145, 1, 32, 44, 209, 2, 0, 44, 177, 4, 0, 244, 65, 6, 0, 244, 65, 6, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0 ] }, { "register": 51, "data": [ 2, 44, 145, 1, 16, 44, 209, 2, 0, 44, 177, 4, 0, 244, 65, 6, 0, 69, 65, 6, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0 ] }, { "register": 55, "data": [ 62, 192, 18, 65, 180, 144, 1, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0 ] }, { "register": 92, "data": [ 204, 4, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 4, 0, 0, 0, 4, 0, 0, 0, 0, 0, 0, 0, 4, 0, 0, 48, 0, 0, 0, 0, 0, 0, 0, 0, 0, 75, 157, 0, 0, 156, 155, 0, 0, 0, 0, 0 ] }, { "register": 112, "data": [ 1 ] }, { "register": 152, "data": [ 1, 0, 1, 0, 2, 36, 143, 36, 143, 170, 6 ] } ] } } }
Thanks,
Jay