This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24295: BATFET, VINDPM clarifications

Part Number: BQ24295

Tool/software:

A few other questions:

  1. When BATFET is disabled either via REG07[5] or at end of charge, there is always some µA current drawn on VBAT (about 8µA). It also seems that VBAT voltage remain sense as VSYS remains linked to VBAT (VBAT+0.15V) or equal to VBAT.
  2. Input power source detection: after initial powerup, what condition will retrig a new power source detection ? VBUS falling under VINDPM REG00[3-6]  ? Others ?
  3. Is there cases where we can be stucked in Input power source detection (DPDM_EN stay to 1, and input power source current limited to 100mA) ?
    • We see this when Vbus is near VINDPM
    • We also have historical casewhere condition are not  exactly known, but disabling/eanbling charger is enought to go out
  4. We have disable BATFET and Watchdog. In some cases (products on field), BATFET is enabled back (only bit REG07[05] is changed). This is not by a REG07[05] write, the only other possibility I see is a pulse on QON, that is floating on our PCB [but has an internal 1Mohm pulldown]
  5. Registers reset: it seems that this reset is not always done when requested. Is there prerequesite ? Will it start a new power source detection ?
  • Hi Emmanuel, 

    Please see my comments below. 

    1) Please refer to Quiescent Currents specifications listed on datasheet page 7. With BATFET disabled maximum Iq is 20 µA. Yes when charge is complete SYS continues to be maintained above VBAT. 

    2) A new power source detection will occur if VBUS falls below V_BADSRC (3.8V typical). VBUS falling below VINDPM will stop the converter, but does not result in new power source qualification and source type detection. 

    3) This case would require additional information, but device is not expected to get stuck in input source detection. If input does not match any adapter types it will be unknown/non-standard adapter.

    Are you initially setting DPDM_EN = 1? Please keep in mind input current is limited when VBUS is near VINDPM in an effort to keep buck converter active. 

    4) The only methods to exit shipping mode are listed in datasheet section 8.3.1.2.2. Considering QON pin is floating in your system the only methods to turn on BATFET are register write to REG07[5] or REG01[7] or an adapter plug in. 

    5) There should not be any prerequisite. To investigate further please show a register dump before and after setting REG01[7] = 1. It will not start a new power source detection assuming VBUS is not removed. 

    Best Regards,

    Garrett

  • Hi Garrett,

    Thanks for this, here are more details:

    1)Ok for VSYS above VBAT

    2 and 3) I've done more tries and have a better understanding. Let me try to explain.


    *In my first try*, there is a confusion between DPM bit REG08[3], that is not related to DPDM detection, but VINDPM (limitation in input due to voltage or current) and true DPDM that should be monitored by reading DPDM_EN (REG07[7]).
    So I have some DPM that occurs, with voltage level that is near VINDPM threshold - but that's only a coincidence, Changing load point, this DPM threashold will change (higher or lower) clearly showing that's in not related to VINDPM threshold but related to IIN DPM limitation.

    In real application (not in my tries) we intially set DPDM_EN at startup. In my memory it was to recover from bad power source detection (for example when there is some glitch during power socket insertion, specifically during product testing).

    ==>Is there any drawback to force such DPDM ?

    I'm also vastly suspecting that I can have such rare unwanted event of new DPDM during some extern power event for example line small glitch power outage of  a few ms to hundred ms. So VBUS must fall below 3.8V during these event and being unstable during detection. [I've not tired to reproduce this at the moment].

    So let say my system is running. It's current consumption is about 110mA to 150mA on VSYS voltage. This current is not highly  dependant of VSYS voltage (but remains a bit) as main power is LDO to 3.3V. Only one part (modem) use a PMIC that will depend of input voltage.

    Input current is fully dependant of VSYS voltage as buck will draw current depending on power.

    VSYS is dependant on VBAT, so with a high VBAT (let say 4.0V), I will drain more current on VBUS. In case of a DPDM, this current will be limited to 100mA during detection, limiting then stopping battery charge, and then lowering VSYS voltage. In turn power consumption will lower and some stable point will be found. But possibily not instantly.

    ==>Will DPDM be disturbed by the fact it enter DPM (potentially dynamically) during DPDM

    I will reply on other points a bit later.

  • Hi Emmanuel, 

    Thank you for the detailed explanation. I am checking on it and will get back to you in the next couple days. 

    Best Regards,

    Garrett  

  • Thanks Garett. I also add a few more question related to "faults"

    Charger faults:REG09 [4-5] 

    01:input fault (OVP or bad source).
    02:thermal shutdown.

    When we see one of these 2 faults, converter stop. After input goes back to good value or IC cool down, do we need to reset the fault to restart converter ? do we need to disable/enable charge to reactivate battery charge ?

    03:charge timer expiration here we must disable/enable charge to restart it

    BATOVP REG09 [3]

    When we see this fault, charge is disabled (REG01[4] goes back to 0 ?), we must reenable it when BATOVP disappear to restart charge ?

  • Hello Emmanuel,

    We are still looking into this and will respond after verifying with others in the team.

    Sincerely,

    Wyatt Keller

  • Hi Emmanuel, 

    Thank you for your patience. Please see my comments below. 

    Is there any drawback to force such DPDM ?

    There is no drawback to forcing DPDM detection with input source already plugged in other than input current is limited to 100mA during the detection procedure. 

    Will DPDM be disturbed by the fact it enter DPM (potentially dynamically) during DPDM

    DPDM detection should not be disturbed by entering DPM during DPDM detection. Input current will be limited to 100mA, so if SYS load draw is large enough device will enter supplement mode where battery discharges to help support SYS load. Once DPDM detection is complete and input current limit is set to a higher value device will exit supplement mode and return to battery charging. 

    When we see one of these 2 faults, converter stop. After input goes back to good value or IC cool down, do we need to reset the fault to restart converter ? do we need to disable/enable charge to reactivate battery charge ?

    You do not need to clear the fault to restart converter and similarly you do not need to disable/enable charge. Assuming charge is enabled converter will start as soon as IC cools down or adapter in valid voltage range is present at input. 

    03:charge timer expiration here we must disable/enable charge to restart it

    Correct, datasheet section 8.3.3.5 lists 4 actions that can be used to restart charge after safety timer expiration. 

    BATOVP REG09 [3]

    When we see this fault, charge is disabled (REG01[4] goes back to 0 ?), we must reenable it when BATOVP disappear to restart charge ?

    The device will resume charging on its own when battery voltage falls back below the battery regulation voltage. REG01[4] will not go back to 0 and there is no need to reenable charge. 

    Best Regards,

    Garrett

  • Garett,

    Thanks for all of this.

    Just 2 lasts questions:

    1)
    >>03:charge timer expiration here we must disable/enable charge to restart it
    >Correct, datasheet section 8.3.3.5 lists 4 actions that can be used to restart charge after safety timer expiration. 

    When timer expire, charge is stopped.
    ==>Does REG01[4] CHG_CONFIG is modified internally at this time ? I had a doubt, but it seems that this bit remains to 1, and I had to set to 0 then to 1

    2)Specific case:

    My battery is at 3.2V
    Charge battery, 102.4mA
    Input limitation: 100mA (@5V)
    VSYSMIN:3.7V
    If I have no load on VSYS, charge will be at 100mA

    A)If my load on VSYS is increasing, charge current will reduce, down to 0mA. In fact we will start to have some low current out of battery (8µA in my case), this is the "quiescent" always present


    B)If my load is increasing more, my VSYS voltage will start to lower. It seems that this quiescent is increasing (12 to 15µA).
    ==>Is this expected ? it remains limited by the "battery discharge current specification" ?
    What I'm searching for is something in range of "1mA" leak (at room temperature) in this kind of very specific case (not general case) we see of one product that ended with a battery issue (I can't fully exclude that DPM is also in progress - but not permanently, juste during load transient for exmaple)

    C)With more load increase, VSYS will reach 3.2V and at this time, we will enter supplement mode, were current drawn on battery will increase to the needed value for supplying VSYS

    When I reach the charge timer expiration, it seems that my 12/15µA load remains (in situation B) ? that seems to be part of quiescent, true ?

    Regards,

    Emmanuel

  • Hi Emmanuel, 

    Please see my comments on your questions below. 

    1)

    Does REG01[4] CHG_CONFIG is modified internally at this time ? I had a doubt, but it seems that this bit remains to 1, and I had to set to 0 then to 1

    REG01[4] 'CHG_CONFIG' is not modified internally due to safety timer expiration. You will want to set bit to 0 then back to 1 to re-enable charge. 

    2) When SYS load is large enough that input supply cannot support it is expected for VSYS to drop below battery voltage to allow battery to discharge and engage in supplement mode. 

    The slight quiescent increase appears to be due to the device being on the edge of needing to transition to supplement mode. The BQ24295 draws slightly increased current from battery because input source has reached input current limitation attempting to regulate SYS above SYSMIN. The quiescent current you observe is within reason given the Quiescent current specifications listed on datasheet page 7. 

    Best Regards,

    Garrett