This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR38025-Q1: LMR38025-Q1 no-load current is very high, i.e., 10 mA.

Part Number: LMR38025-Q1


Tool/software:

We are using LMR38025-Q1.

The no-load current is very high, i.e., 10 mA. Below are the key values of components

  • Input Voltage: 24 V
  • Switching frequency = 400 kHz
  • Inductor L1 = 15 uH
  • R FBT = 50K
  • R FBB = 10K
  • RT =64.9K
  • Series resistor for PG = 10K

Is it because of FPWM mode? 

  • Hello Kapeesh,

    Thank you for posting.  The experts of this device are currently out of office.  I studied the datasheet and I think you are right about the FPWM mode.  If you want to achieve low Iq under no load, please use the PFM mode version of the device. 

    Hope this helps.'

    Regards,

    Youhao