This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76952: 1M ohm resistors decreased on PCB

Part Number: BQ76952


Tool/software:

First of all, hello. First of all, I had a problem with the circuit I made and wanted to get your opinions. I cannot get the resistance values ​​I planned. After soldering a 1M resistor to any PCB using flux with a soldering iron, its value decreases. This decrease in value starts when I first put it on and decreases significantly within 5 minutes. And the resistance values ​​are not stable, sometimes increasing and sometimes decreasing. Is the problem with my PCBs? Because when I connected the resistor to the cable instead of the PCB, its value decreased. As I added in the attachment, I use 6 pieces of 1M ohm resistors in the circuit. What they all have in common is that they are connected to a 5 volt voltage regulator. Normally, if the resistors appear to be 1M, 5 volts come out of the resistor in a very healthy way. However, the 1M resistors I put seem low. Although some may seem like 1M, some give values ​​like 100k-300k. In this case, 5 Volts entering from one end of the resistor drops to the range of 1-3 Volts when it exits the resistor. (If there is a 1M ohm floating resistor, things work normally. I tried to explain the situation as clearly as possible in the photos I added. I ask for your help and advice. What could be the reason for this situation and what can be done?) you propose to solve this situation.

  • Hello,

    A few questions:

    1. What is your full configuration?

    2. Why are you using 1MΩ resistors?

    3. Are you trying to use SPI?

    Best regards,

    Thomas Rainey

  • Hello Mr. Thomas,
    Actually, the integrated circuit of the circuit I wanted to make was different from the one I mentioned above.
    Yes, I am trying to use 1M resistors for communication via SPI. But as you can see in the circuit, I could not use it as 5 volts because I could not get a stable resistance value. The reason I use 1M is the resistance value I obtained from the preliminary uses of the integrated circuit I use.

  • Hi,

    Can you clarify the how  of these 1MΩ resistors? SPI communication does not use pull up resistors. SPI uses push-pull drives instead of open drain.

    Best regards,

    Thomas Rainey