This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi Team,
This is Gree FAE Ryker. Recently Gree wants to find a high-power BUCK as below request. Does the LM5149 suitable for these request? And do we have more suitable devices? Thanks.
Best Regards,
Ryker
Hi Ryker,
Yes, the LM5148 (no AEF) or LM5149 (with AEF) 80V current-mode controllers are options here. Also consider the LM5145 75V voltage-mode controller (higher gate drive level for faster switching).
--
Tim
See the LM5146 EVM https://www.ti.com/tool/LM5146-Q1-EVM12V, which is 12Vout, 8A, 400kHz and quite close to the customer's spec. The LM5146 is the same as the LM5145 but rated for 100V input instead of 75V.