This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61378-Q1: TPS61378 No output issue

Part Number: TPS61378-Q1


Tool/software:

 Team,

Currently my customer finds that there is one TPS61378 no output. The input voltage is 7.7V and normal board output voltage is 125V. On one board, we find that the Vout=0 and OUT=8V, SW output is good and no short-circuit in OUT-GND. We are wondering if the OCP protect MOS is damaged. Is there any way to probe to see if the MOS is damaged?

We can have offline email to discuss based on customer SCH if needed. Thanks.

Regards,

Jason