This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65219: Is there any risk when Vbais set 1.0V?

Part Number: TPS65219

Tool/software:

Hi TIer

Customer use tps6521901 asPMIC for AM6254.

Customer have to set Vbais is 1.0V due to some issue.But in datasheet the recommended value is 1.5V at less.

So is there any risk for this setting?

Do we have some pin2pin solution which support 1.0V bais ?

Customer need some more convenient way to modify. Thank you very much.