Tool/software:
About this evaluation board: Design of LMG3626EVM-074, which uses a transformer RLTI-1454
This transformer is on the evaluation board: LMG3626EVM-074 Can you provide me with the manual so that
I can customize this transformer one by one, because only RM8 can be seen in the schematic diagram?
200uH 6:1 Lack of residual information, including transformer skeleton, primary, secondary,
auxiliary stage windings, winding turns and wire diameter of these information,
can provide complete information