This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPSM83100: How much current can I get if using single cell li-battery boost to 5V?

Part Number: TPSM83100

Tool/software:

Hi :

I want to use TPSM83100 to boost to 5V with single cell li-battery in my design.

The system should be power off when battery voltage is less than 3V, so the input of TPSM83100 is 3V~4.2V.

The question is as thread title, I need 5V/1A for my design, can TPSM83100 use for my design or not?

And can you tell me the max current I can get from my design?

By the way, the inductor in TPSM83100 is 1uH?