This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25731: feasability very low charging current <300mA

Part Number: BQ25731

Tool/software:

Hello Team, 

my customer currently evaluates the part for his project. Can you please help to understand if the device works in the customer application.  

Values Based on 5x Panasonic BK3 10 CH for the BQ25731

Inductor Selection

 

 

 

ICHG

Charge current

333

mA/Pack @ 5 Cells

IRIPPLE

Inductor current ripple peak-to-peak value

2930

mA

ISAT ≥ ICHG + (0.5)IRIPPLE

Minimum Saturation Current of the Inductor

1798

mA

VIN

Input Voltage to the Charger

24

V

VBAT

Maximum Battery Charge Voltage

7,5

V

VOUT

USB OTG Output Voltage

24

V

POUT

USB OTG Maximum Power Output

20

W

fS

Switching Frequency

800

kHz

L

Inductance

2,20

µH

DBUCK = VOUT/VIN

Duty Cycle Buck

0,31

 

IRIPPLE_BUCK = VIN × DBUCK× (1-DBUCK) / (fS × L)

Inductor Ripple Current in Buck Mode

2930

mA

DBOOST = 1 – (VOUT/VBAT)

Duty Cycle Boost (USB OTG Boost Converter)

0,69

 

IRIPPLE_BOOST = (VOUT × DBOOST) / (fS × L)

Inductor Ripple Current in Boost Mode

2930

mA

η

efficiency of the Buck Converter

80

%

IL(DC_MAX) = (VBAT × ICHG) / (VIN ×  η)

Max DC current

130,21

mA

η

efficiency of the Boost Converter

90

%

IOUT(MAX)

Maximum Supply Current from BMS

833

mA

IL(DC_MAX) = (VOUT × IOUT(MAX)) / (VIN ×  η)

Max DC current

2963

mA

Safety Factor

Aditional margin for component ratings

50

%

ICIN_BOOST = ICHG × √(DBOOST × (1 - DBOOST))

 

154,50

mA

 

 

 

 

 

 

 

 

 

 

 

Inductor Values

 

 

L

2,2µH

 

 

ISAT

> 2700mA

 

 

IL(DC_MAX)

> 4440mA

 

 

This is the configuration with the highest charging current, there is also a 3
cell application for the same board, which has only 200mA charging current. As inductance we have chosen this Würth coil: 7440700022

Let me know if you need more information!

Thanks 

Jan