Other Parts Discussed in Thread: TPS92620-Q1, LM3409, TPS92692
Tool/software:
Greetings,
I'm facing current drop issue when i increase the length of the cable,
92 LEDs are consuming 1.5A of current with 30cm cable but when i increase the length of the cable huge amount of current drop is there..
for 1 meter all LEDs 1.3A and with 5 meter cable current consumption is 1A.
single LED's forward voltage is 3.2V
Also please tell me till how much length of the cable can TPS92612 drive ?
please give me any solutions, i have be tried multiple types of cables but observed the change only ±10mA difference..
Best regards,
Tex