Other Parts Discussed in Thread: BQ25750, LM74930
Tool/software:
Hi!
I have drone project.
It has Fuel cell and 12s-14s battery.
Battery is needed to provide high curent (up to 300A) to the system, when fuel cell can provide only 50A.
Battery should give power automatically when fuel cell goes down (ideal diode lm5050 selected for this role)
Battery should be charged in flight (up to 20A)
Here are current schematics

I think to add BQ25756 as standalone charger from fuel cell
But it looks like BQ25750 can solve all my problems, at least it can remove TPS48110 as switch, it would be nice if it can remove also LM5050.
All I need - auto switch when fuel cell loses power to battery, and I am not sure if BQ25750 has internal engine to do so.