This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ79616EVM-021: Questions about BQ79616 EVM

Part Number: BQ79616EVM-021
Other Parts Discussed in Thread: USB2ANY, BQ79616

Tool/software:

Hello TI team,

I have started setting up the BQ79616-EVM with USB2ANY for the cell monitor. I have two questions:

1- The "Wake Up" button in the GUI turns on the green D1 but the device keeps disconnecting every-time clicking "Auto-Address". The cell voltages are not appearing. I am testing with S1 and S2 closed (resistor ladder closed) and +18V between STACK and GND. THe J17 is connected to USB2ANY and to the USB port of PC.

2- Second question: I cannot find the example code for communicating between BQ79616 EVM to TMS570. It says it should be requested from the product page but it hasn't been easy to find it. How should I request the example project to receive in my secure resources section?

Thanks a lot,

Farshid