Other Parts Discussed in Thread: BQSTUDIO
Tool/software:
Hello,
Currnet my 'battery' (power supply connected currently) is showing 0%
1)How do I reset the charge to someting arbitray like 90%?
2)I'm trying to configure interrupts. In my reading soc delta = 0, implies rsoc interrupts are off. Though on the bqstudio I set SOC Delta = 0, write, and then if i reset it goes back to one. I do not see the interrupt clear. How do I turn this off through the gui?
After further experimentation soc delta ON THE GUI is not sticky. Looks like it doesn't write to flash. Thus you can't disable it.
I was able to manually write to flash with my own code and disable it. This is the only way I could disable the interrupt.
Likewise the io Config does not appear sticky either...
mmmm...actually might of been below flash write voltage...