This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM76005: LM76005 high Vin

Part Number: LM76005
Other Parts Discussed in Thread: LM70840

Tool/software:

If I want to convert 58V to 10V, 4A, the Vin will up to 59.5V, but it never reach 60V, 

pls help evaluate if LM76005 can withstand this high Vin, the datasheet shows 65V is the Absolute Max rating. 

Pls recommend a part if it can't meet his requirement. Thanks. 

Alex