Tool/software:
Hi Ti
When I was designing the TLV61220, I found that the quiescent current at the input end of the chip is too large, when Vin=1.2V, Vout Noload, the input current is about 25uA when tested with Powermonitor.
At the same time, I also applied for the TLV61220EVM-120 comparison test, VIN=1.2V, Vout Noload, the quiescent current of the EVM tested with Powermonitor is also 29uA, but the theoretical current described in the specification is only 5uA, I want to ask what is the reason for this?
The figure below shows the TLV61220EVM-120 quiescent current test data
The figure below shows the parameters that are submitted in the datasheet