This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7A24: Could I change the current limit(ICL)

Part Number: TPS7A24


Tool/software:

Hi TIer

Currently , My customer used MIC5205-5, I searched TI chip and TPS7A24 is good alternatives.

Customer need output 5V input is 5.5V±5% , max output current is 150mA. 

Noise,PSRR and Load regulation at least higher than MIC5205-5

Customer need When the LDO is shorted, the output current is limited to approximately 200 mA. The customer's load is dynamic, 100mA max.

I see that the ICL of the TPS7A24 is up to about 600mA, which doesn't meet the user's needs, do we have a way to change the ICL? Or can I recommend another chip that is more suitable

Thank you very much.