This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65987D: Working with Xiaomi but not with Samsung S8 or A8 with as UFW and Power source

Part Number: TPS65987D

Tool/software:

Hi TI,
Our Config is UFP (LAN 7800 Device controller) + Power Source (5V 3A). TPS65987D as a PD controller. Working with Xiaomi but not with Samsung S8 or A8(only power is going but not internet or data) but we can see the led blinking with the Ethernet port.


This is the project file

DRP_UFP_PS.pjt