Tool/software:
Hi TI Team,
The LM74502, LM74502H SNOSDE5A datasheet revision A Section 9.3.3 suggests "An additional zener diode from GATE to SRC can be needed to protect the external FET in case output is expected to drop to the level where it can exceed external FET VGS Rating."
Assuming the External Fets have a VGS Max of +/-20V:
Could you explain what condition or case would cause the LM74502 Gate to Source voltage to exceed the external FET VGS rating?
What specification should the zener diode meet?
Regards,
Jim